Skip to main content
YK Choi and Youngjae Kang image image

Presentation

Designing 48V zonal architecture that keeps the high voltage inside the BEV battery pack

The future BEV systems will be required lots of heavy loads and safety system with 12V legacy power. Generally BEV has double layer power structure, but when OEMs adapt zonal architecture the system requires triple layer power with additional 48V. The most of DC-DC converters in vehicle have standard power rate, it's simple to increase power demand by add one or two dc-dc converters in vehicle, it’s possible but how we can deal the volume of dc-dc converters and wire harness in system.

YK Choi

Sr. Field Application Engineer, Vicor, APAC

YK Choi is Senior Field Application Engineer at Vicor, APAC. YK has over 26 years of experience in power electronics, power modules (IGBT, SiC), discrete switches and semiconductors. He has expertise in vehicle electrification based on traction inverter systems. Mr. Choi has held positions as an R&D engineer and as a field applications engineer in semiconductor test equipment and has also worked at Infineon Technologies. He has MS in Power Electronics and BS in Electrical Engineering from Konkuk University in Korea.

Photo of YK Choi

YoungJae Kang

Chief Engineer, INFAC Corporation

Youngjae Kang has over 20 years of experience in the structural and automotive industry. He is a Chief Engineer at Infac, based in their Michigan office. Youngjae’s mastery and expertise lies in CAE analysis and structural analysis. Dr. Kang has earned a Ph.D. in Structural Engineering from University of Michigan, and an M.E. and B.E. in Civil Engineering from Kyunghee University in Korea.

Photo of Youngjae Kang

Originally presented at World Congress Expo on April 17, 2024