Skip to main content

World’s first commercialized hydrogen fuel cell powers drones for humanitarian missions

Media Alert

Powering Innovation: World’s first commercialized hydrogen fuel cell powers drones for humanitarian missions

January 12, 2021

Solar panel inspection is achieved with far great efficiency and speed by DMI drones.

Solar panel inspection is achieved with far great efficiency and speed by DMI drones.

Doosan Mobility Innovation (DMI) is delivering humanitarian relief to remote locations using drones powered by its innovative energy-dense hydrogen fuel cells. With two hours of flight time, the drones have transported masks and emergency supplies between US Virgin Islands and have delivered medical AEDs to the top of Mt. Hallasan (6,388 ft), the tallest mountain in South Korea located on Jeju Island. This technology paves the way for developing mobile robots with extended range and load capacity.

Vicor-case-study-doosan-medium.jpg

DMI drones delivered emergency medical supplies to the Virgin Islands. A hydrogen fuel cell power pack made this possible by enabling over two hours of UAV flight time; four times longer than most battery-powered drones.

Additional uses for the DMI extended-range drones have been in commercial applications where longer flight times have enabled the monitoring of vast solar farms such as Korea’s largest solar energy plant in Solasido, Haenam. When performing the same mission using a battery-powered drone, more than six battery replacements were required.

High-density power design to optimize power pack performance

Developing a hydrogen fuel cell for mobile devices requires overall technological innovation from materials science to full system-level design optimization. The key to mobility is miniaturization, increasing efficiency and lowering system weight. Moreover, high energy output and durability should be incorporated for a long, stable flight. Therefore, it is necessary to reduce the weight of the stack, configure a powertrain with high power density and simplify the design of the overall power pack, including peripheral components, to fully optimize the system.

Core to these design goals is the architecture and implementation of the systems power delivery network (PDN). The DP30 power pack has two main powertrains that supply power to the drone’s rotors and to the controller for the two stacks. Because of the wide range and variable output voltage of the DP30 power pack, from 40 to 74V, the powertrains were designed to ensure a tightly regulated 48V, 12A output to the rotor motors of the drone, plus a 12V, 8A output to the stack controller board and fans.

Vicor-Power-Energy-System-Doosan.jpg (Vicor-Doosan-Energy-Density-Chart)

Energy density comparison: hydrogen fuel cell vs. lithium power

To achieve high efficiency and high energy density in the PDN, DMI selected Vicor PRM™ buck-boost regulators and a ZVS buck regulator. The PRMs support the up to 74V open circuit voltage (OCV) of the hydrogen fuel cell stack and perform a stable voltage regulation to 48V.

Media-alert-doosan-fuel-power-diagram-small.jpg

Structure of hydrogen fuel cell power pack

In the drone’s rotor-side PDN, two PRM buck-boost regulators (PRM48AF480T400A00) are configured in parallel to supply the 12A required by the rotors. The PDN for the digital controller board in the stack, uses a lower-power PRM (PRM48AH480T200A00) followed by a 48V-to-12V ZVS buck regulator (PI3546-00-LGIZ).

Diversification of product lines by power capacity

Apart from the 2.6kW DP30 power pack currently being produced, DMI plans to diversify product lines by power capacity. The company is expected to develop products with various capacities, ranging from the 1.5kW hydrogen fuel cell power pack that is scheduled to be released next year to a 10kW one, and to launch corresponding drones suitable for each power pack.

The Vicor modular approach to power enables scalability to support such diverse product lines. This also allows DMI to focus on solving other engineering problems, such as stack structure changes, powertrain and peripheral components and heat dissipation method, all of which arise from the expansion of power capacity. With Vicor, DMI is better able to pursue its main objectives: to increase durability and stability as well as achieve the miniaturization and lightening of fuel cells with high energy density.

Learn more about Doosan Mobility Innovations’ hydrogen fuel cell power pack.

About Vicor

Vicor Corporation designs, develops, manufactures and markets modular power components and complete power systems based upon a portfolio of patented technologies. Headquartered in Andover, Massachusetts, Vicor sells its products to the power systems market, including enterprise and high performance computing, industrial equipment and automation, telecommunications and network infrastructure, vehicles and transportation, aerospace and defense. www.vicorpower.com

Vicor and PRM™ are trademarks of Vicor Corporation.

About Doosan Mobility Innovation

Doosan Mobility Innovation (DMI) is a subsidiary of Doosan Group, one of the leading global companies in the hydrogen fuel cell market. It was established in 2016 to develop hydrogen fuel cells for mobile devices. Doosan Group has built a complete technology, supply, and production system ranging from materials to systems in the markets of the phosphoric acid fuel cell (PAFC) for 50 years and solid polymer electrolyte membrane fuel cell (PEMFC) for 30 years, supplying fuel cells for automobiles, households, power generation, and buildings. Meanwhile, DMI has focused on the development of hydrogen fuel cells for mobile devices based on Doosan’s proven hydrogen fuel cell technology and various experiences in the stationary applications sector. Moreover, it contributes to the development of the unmanned aerial vehicle (UAV) industry, such as drones and drone taxis. For more information, visit www.doosanmobility.com.