High‑performance PCB layout and thermal design
In cities you’ll often see large full-color LED video displays used for advertising that cover the sides of buildings. With each pixel of the display driven separately, there are challenging demands on the power systems used to convert AC power into the constant current needed to drive the LEDs.
These systems have demanding requirements for the power components they use. Power system cost is an obvious issue, with a large number of power components required to create one of these displays. It’s not surprising that efficiency is also a concern, as the electricity consumed is a key element of running costs and advertisers do not want to be portrayed as wasting money.
The reliability of LEDs decreases with temperature, meaning that if the heat dissipated by the power systems can be reduced, then the lifetime of the LEDs can be extended. It is also often possible to run the LEDs at higher intensity, increasing the brightness of the display. Heat can also change the intensity and the wavelength of the LEDs’ output, resulting in inconsistent illumination across the display.
Power components used in these systems must also operate reliably, whether in direct summer sunlight or in the middle of a winter snowstorm. Failures are particularly expensive due to the cost of repairing or replacing modules that are attached high on a building. As with architectural lighting applications, the costs and dangers of having someone replace parts at height far outweighs the cost of the replacement module.
Perhaps surprisingly, size is also an important criteria. These displays have to be thin to ensure they are mounted as close to the building as possible, and unnecessary weight can also add to the cost of deploying these displays.
Vicor power components are ideally suited to these applications, due to their power density, efficiency and reliability. Recently, we’ve seen customers choosing our 48V Buck Converters, which were recently named one of EDN’s Hot 100 Power Components, to help them achieve their design goals. By offering a compact and efficient 48V direct to point-of-load conversion solution, they allow manufacturers to distribute power in these systems using a SELV 48V bus.
Today most displays distribute power using AC mains to each panel. This approach offers several downsides compared with the use of 48V: there are significant safety considerations associated with the use of mains voltages, and the losses in the AC-DC conversion generate heat that will affect the lifetime, brightness and color produced by the LEDs.
By converting directly from 48V, designers of large displays are able to simplify their power chains, reducing the number of stages, components required and cost of the system, while increasing the efficiency. Vicor Buck Converters make the displays reliable and easier to install, cutting the cost of installation and maintenance.
Related content
Product overview: 48V Buck Converter
Industries and innovations: LED lighting
Vicor power components, ZVS Buck family
High‑performance PCB layout and thermal design
Modular DC-DC system design done right
Edge computing leverages modular power in scalable micro data centers
Optimizing power delivery networks