Skip to main content

White Paper

Back to basics: Choosing the perfect regulator

A voltage regulator provides two functions: changing the input voltage to a different level at the output and regulation (maintaining a constant output voltage despite changing load conditions). DC-DC regulators are a key component in any power system, and so choosing the correct regulator is critical if an optimum solution is to be developed.

Although engineers understand regulator functionality, less experienced engineers often find it difficult to identify the best regulator for their application. This blog post identifies criteria that anyone who is not an experienced power developer can use to ensure they choose the perfect regulator.

Buck, boost or buck-boost regulator?

There are three basic categories:

  • Buck – regulators with an output that is a lower voltage than the input
  • Boost – regulators with an output that is a higher voltage than the input
  • Buck-boost – regulators that can supply output voltages that are higher, lower or the same as the input

In most applications voltages are stepped down from the bus to the load and therefore buck regulators are commonly used. Other applications require the voltage to be increased with a boost regulator: for example, if DC power must be transmitted using a long cable, the I2R losses can be reduced by boosting the voltage before transmission and then stepping it down again at the load. In battery applications buck-boost regulators are often used to provide a constant stable voltage, overcoming the change of output voltage that is seen as batteries charge and discharge.

Nominal inputs and outputs

Many systems have clear requirements for input and output voltage – for example, you may need to step down a 12V rail to 3.3V. For many applications, there will be a suitable regulator available off-the-shelf to meet the voltage requirements.

Obviously, the regulator must be able to deliver the power required by the load. Regulator power is typically specified by a maximum output current.

Input and output ranges

Although applications often require a specific voltage, others will require an adjustable output. This might be because the loads change – for example in a piece of test equipment – or it may be that the load is supplied by a long cable, and the voltage needs to be trimmed a little higher than required by the load to compensate for the voltage drop across the cable.

Input voltage ranges are particularly important for applications such as battery-powered systems. In an automotive application, a nominal 12V battery might deliver 12.5V at full charge and drop to 10V or less as the battery discharges. A regulator with a narrow input range may no longer function as the battery voltage drops, meaning that the full capacity of the battery cannot be used. Ensuring a sufficiently wide input range is therefore an important criterion for selecting your regulator.

Choosing wide input regulators also has another benefit: they can also reduce inventory costs as a single regulator can be used in a variety of different situations.

Battery-Output-Voltage-Variations.jpg

Efficiency

Efficiency is one of the criteria for most power systems designed today. Selecting a regulator with high power losses can make it almost impossible to meet efficiency goals. It’s important to also remember that regulator efficiency is not constant: typically, the efficiency of the regulator will fall dramatically as the step-down or step-up ratio increases and as the current drawn from the output decreases.

Modern regulators, such as those based on Vicor’s Zero Voltage Switching (ZVS) topology offer inherently high efficiency and are more consistent across the whole operating range.

Noise

Switching regulators provide high efficiency, but the switching circuit generates noise. In some systems, particularly those with sensitive analog components, the power supply noise can limit overall performance. Unnecessary electronic noise can also make it more difficult to achieve EMC certification.

As with efficiency, the regulator topology is key to achieving low noise: it’s much easier to use a component that doesn’t generate noise than it is to try to filter that noise out. ZVS, for example, is a soft-switching topology that is inherently low-noise, making it easier to develop high-performance systems.

Size and packaging

Today electronic systems are often space constrained. Even if the goal is not to make the system as small as possible, such as products housed in standardized 19” rack units, reducing the size of the power system allows the space saved to be used to add additional functionality.

Any calculation of size should also consider the peripheral components required by the regulator. With higher levels of integration and high switching frequency, the size and number of peripheral components can be reduced, which can potentially offer a greater space-saving than simply picking a regulator in a smaller package.

The package types available don’t only determine the space required: often smaller packages can be located closer to the load, enabling more accurate regulation at the load and faster transient response.

In addition to size, weight can also be an important factor, particularly in applications where the equipment can move. Examples of such systems range from hand-carried portable equipment to automotive electronics and drones.

Operating temperature & thermal performance

Regulators cannot be 100% efficient, so they will always dissipate heat that must be removed. If a heatsink is required, this can significantly increase both the size and weight of the power system. Failure to dissipate heat can also impact the system performance in other ways: for example, in lighting or display applications if the regulator causes an increase in temperature of the LEDs, this will reduce the intensity and change the wavelength, and therefore the hue, of the light generated.

The regulator must function reliably across the range of temperatures to which it can be exposed. In general, more efficient regulators will be able to operate at higher temperatures, as they do not need to dissipate so much heat, but products from different suppliers can vary widely so it is important to check the data sheet.

Additional features

In addition to the criteria described above, your application may require some specific functionality, which can limit choice. Examples of these additional features include:

  • Paralleling capability: if regulators can be paralleled, then higher output currents can be delivered. Not all regulators can have their outputs paralleled, as with many topologies this will cause instability.
  • Constant current output: in battery applications, a constant voltage is needed to supply the load, but constant current is required for charging. Some regulators offer outputs that can be configured both as constant current and constant voltage, making them ideal for these systems.
  • Soft start: the ability to ramp up the voltage slowly helps to ensure the power system is stable, even when large amounts of capacitance are connected to the output of the regulator.
  • Overvoltage protection: regulators that have protection to ensure they cannot deliver more than the defined output voltage ensure that the load will not be damaged even during a fault. Other protection circuitry might disable the regulator if the input voltage is out of range.
  • Transient response: some loads rapidly change the current they demand. A fast transient response ensures that the regulator can deliver the power needed, without large output capacitors to store energy.

Conclusion

Although regulators are conceptually simple components – they take a voltage at the input and deliver a different voltage at the output –  there are many factors that determine the best regulator for your application. Carefully considering the criteria outlined above will help to ensure you pick the ideal regulator for your system.

Related content

Product overview: ZVS regulator evaluation board

Product overview: ZVS buck regulator

Product overview: ZVS buck-boost regulator

Resources

Contact Form

Get in touch with Vicor

Thank you for contacting us

You should receive a reply to your request within one business day.