Saab UK innovates deep-sea exploration mitigating risk to divers and the environment .
Saab UK innovates deep-sea exploration mitigating risk to divers and the environment
High-density power modules support world's first work-class, all-electric ROV

Figure 1: Saab has developed the world's first work-class all-electric ROV (eWROV), which combines versatility and maneuverability. Unlike traditional hydraulic ROVs, the eWROV all-electric system eliminates the need for large amounts of hydraulic fluid, thereby mitigating environmental risks.

Figure 1: Saab has developed the world's first work-class all-electric ROV (eWROV), which combines versatility and maneuverability. Unlike traditional hydraulic ROVs, the eWROV all-electric system eliminates the need for large amounts of hydraulic fluid, thereby mitigating environmental risks.
Less than two years ago, two Saab remotely operated vehicles (ROVs) descended over 3,000 meters into the frigid Antarctic waters in search of Sir Ernest Shackleton’s ship, Endurance, which sank in 1915. The story of the British explorer is a legendary tale of courageous leadership and perseverance. Saab’s Seaeye ROVs were integral to the mission’s success, using sophisticated technology to locate, examine and film the wreckage, thus eliminating the need to endanger human lives for deep-sea exploration
Historically, commercial divers have taken great risks to inspect oil and gas pipelines, high-voltage electrical cables, wind turbines and other critical infrastructure deep undersea. Saab has eliminated that risk bringing deep-sea exploration expertise to on commercial underwater applications.
With a mission to keep people and society safe, the Seaeye range of ROVs has been developed with more agile and modular systems designs. Saab UK’s Seaeye systems are capable of performing a wide range of tasks from observation and inspection to more complex functions like underwater maintenance.
This evolution has culminated in the development of the world's first work-class all-electric ROV (eWROV), which combines versatility and maneuverability. Unlike traditional hydraulic ROVs, the eWROV eliminates the need for traditional hydraulic fluid, thereby mitigating environmental risks.
eWROV: all-electric ROV
With a burgeoning ocean economy, Saab’s eWROV competes with traditional hydraulic ROVs, delivering performance equivalent to a 250hp undersea vehicle. The eWROV uses limited hydraulic systems and environmentally-friendly oil, which removes the risk of accidentally discharging pollutants into the ocean that can harm the surrounding ecosystem.
The move to electric propulsion comes with several additional benefits. First, reliability vastly improves with fewer high-pressure systems. This also improves the service interval, allowing for longer operating periods and self-monitoring for less routine servicing.
Power density: a competitive advantage
The advanced features in Saab’s eWROVs are largely achieved by their exceptionally high power density, which adds significantly more payload space while outperforming larger, hydraulic ROVs.
Figure 2: A more efficient and environmentally-friendly system makes the eWROV the world’s most capable and intelligent all-electric, work-class underwater vehicle.
By maintaining a constant subsea voltage level, the DC power system optimizes energy delivery to the ROV's components, reducing overall energy consumption from surface power systems. Consequently, lower energy demands lead to decreased CO2 emissions from surface power generation, making operations more environmentally friendly.
High-density modular power achieves a compact scalable design
Critical specifications for the eWROV’s power converter are size, mass and thermal dissipation, given that the electronic systems are housed in sealed enclosures where space is at a premium and conventional convection cooling is not possible.
To meet these requirements, Saab chose Vicor power modules for their high density and efficiency. These modules enable efficient power distribution to various eWROV subsystems such as thrusters, manipulators and onboard electronics. The use of Vicor power modules allows Saab to customize Seaeye subsystems according to specific industry-standard 24V and 48V levels required by onboard computers, sensors, video cameras, lights and navigation equipment.
Saab has been an innovator since 1937 with a mission to “keep people and society safe.” This next-generation eWROV is the model for the industry, with its high-performance power delivery network design that helps drive ROV designs that can still handle heavy power loads. Saab’s innovative hybrid approach to design and operation is further solidifying the company as a global leader in ROV products and services.
Learn more about Saab Seaeye, the world’s first eWROV.
About Vicor
Vicor is the leader in high-performance power modules, enabling customer innovation with easy-to-deploy modular power system solutions for power delivery networks that provide the highest density and efficiency from source to point-of-load. We continuously advance the density, efficiency and power delivery capabilities of our power modules by staying on the forefront of distribution architectures, conversion topologies and packaging technology. Vicor serves customers in enterprise and high-performance computing, industrial equipment and automation, robotics, UAVs, electric vehicles and transportation, satellites, and aerospace and defense. www.vicorpower.com
Vicor is a registered trademark of Vicor Corporation.
About Saab UK
Since Saab was started, we have striven to keep people and society safe. It is a basic human need to feel safe and, as we see it, a human right. Through systems and solutions that increase security, we can make this possible.
When Saab was founded in 1937, our primary aim was to provide military aircraft for Sweden. Today, we serve the global market with world-leading products, services and solutions from military defence to civil security. With operations on every continent, Saab continuously develops, adapts and improves new technology to meet customers’ changing needs. Saab UK.