MHz switching frequency-based devices enable miniaturization of the DC-DC converter and EMI filters
Imagine using DC-DC converters solutions to harness the benefits of high-frequency switching without incurring conventional shortcomings
A key factor in designing high-density power devices is the thermal performance of the internal circuitry. Vicor maximizes efficiency to reduce the losses as far as possible when designing these devices. Even so, the heat generated by residual losses must be dissipated to avoid overheating, which has a direct impact on reliability.
As with the electrical test equipment, much of the all-important thermal testing equipment has been developed by the Vicor R&D department. The sophisticated wind tunnel system is one of the best available on the market, but the specialized thermal measurement equipment, product interfaces, specialized thermocouples and analysis systems are all designed and built in-house.
All test stations, and many non-production ATEs, include sensitive thermal cameras to identify potential hot-spots within the device to ensure the product does not exceed the thermal parameters under all load conditions in order to maximize performance, density and reliability. This detailed thermal analysis, extensive burn-in and the subsequent test data obtained is also used as a direct feed for Vicor comprehensive data sheets.
Vicor considers its high level of investment in design and testing essential to ensure that comprehensive, real-world data are obtained. Investment in development and tools is a top management priority within the company; every operation is equipped to do the job thoroughly. The company’s R&D budget is a high priority and is funded generously as part of the company’s strategy to invest in innovation.
In addition to the accuracy and detail of product datasheets, the investment also means that customers benefit from the many tools and resources available from Vicor. The Vicor suite of tools includes a web-based comprehensive solution selector that enables customers to select the best product for the application together with simulation to show exactly how the product behaves under all conditions. The Whiteboard helps customers configure their own optimized system solution, allowing them to simulate and evaluate performance at a power system level. Test date from real devices is used as the data feed for tools like the Whiteboard ensuring very high accuracy.
Wind tunnel used for thermal testing
Orthogonal thermal conductivity matrix representation of PCB trace and via geometry
MHz switching frequency-based devices enable miniaturization of the DC-DC converter and EMI filters
Imagine using DC-DC converters solutions to harness the benefits of high-frequency switching without incurring conventional shortcomings
Future-proof advanced EVs by adopting 48V zonal architectures
As OEMs move to 48V, they consider how to optimize their power system design. Vicor power-dense modules deliver peak efficiency for 48V Zonal Architectures
A novel way of using power modules to eliminate electric vehicle high-voltage pre-charge circuitry
With a dense power module, engineers can design novel architectures that balance the tradeoffs associated with vehicle pre-charging
Reducing EV weight with high-density power modules
EVs have a weight problem. Vicor high density power modules combined with a 48V zonal architecture can significantly cut weight and improve efficiency.