High-density, high-power modules enable lighter, safer, lower cost tether cables to extend missions
This class of unmanned vehicle is powered and controlled via a tether from a ground-based power source assisting in extended missions
Robotics solutions and case studies
Case study: Medical knee surgery robot
Reducing the scale of any intervention is a common aim in surgery, enabling the patient to recover more quickly. Miniature robotic tools can facilitate a reduction in the scope of the surgery. In addition, linking the position of the tool to a patient’s CT scans improves precision and reduces risk. Reducing the surgeon’s fatigue requires the minimization of the size of hand-held operat-ing tools. This manufacturer had the twin goals of reducing the weight of their hand-held robotic tool and improving its reliability. The key goals were:
Power for the tool came from a 55V medically isolated bus and required conversion to 24V within the tool to drive the motors and control circuitry. To save space and weight a DCM DC-DC converter was selected that provided the 300W required in a footprint of just 8.8 cm2 and a weight of only 24g. The converter featured a low noise switching topology and also provided isolation, helping to reduce EMI from the device. Key benefits were:
A DCM DC-DC converter converted the 55V input to 24V 300W to drive the motor and control electronics. The high efficiency (91.3%) of the converter reduced waste heat in the tool, improving system reliability. To analyze this power chain go to the Vicor Whiteboard online tool.
High-density, high-power modules enable lighter, safer, lower cost tether cables to extend missions
This class of unmanned vehicle is powered and controlled via a tether from a ground-based power source assisting in extended missions
High-efficiency, high-density modules free up space for advanced communications and extend range
High-efficiency class of UAV depend on solar power to meet its long flight time requirements
DCM DC-DC converters double the internal bus power and help keep the aircraft as light as possible
High-altitude long-endurance (HALE) UAVs are essentially flying satellites, designed to operate at extremely high altitudes for extended periods
Lightweight and efficient power modules extend delivery routes and save space to carry more goods
Last-mile consumer delivery of groceries, take-out food and online consumer items is the mission-critical task of autonomous robots